Compile error when make i.MX Yocto project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compile error when make i.MX Yocto project

4,885件の閲覧回数
okado-tomohiro
Contributor I

Hi,
I am using the imx 6Q SABRE-SDB development board. I want to download and build the i.MX Yocto project following the i.MX Yocto Project User's Guide, Rev. L4.9.88_2.0.0-ga, 05/2018.
But it report an error when executing "bitbake fsl-image-machine-test" command. The host environment is ubuntu 18.04 LTS on vmware. I don't know why it report the error. I have tried several times and the error remains.
 

Please tell me how resolve or avoid this problem. Thank you.

The error log is as following,

okado@ubuntu:~/imx-yocto-bsp/build-x11$ bitbake fsl-image-machine-test
WARNING: Host distribution "ubuntu-18.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |########################################################################################################################################################################| Time: 0:00:03
Loaded 3262 entries from dependency cache.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:00:04
Parsing of 2423 .bb files complete (2421 cached, 2 parsed). 3264 targets, 207 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "1.36.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-18.04"
TARGET_SYS           = "arm-poky-linux-gnueabi"
MACHINE              = "imx6qsabresd"
DISTRO               = "fsl-imx-x11"
DISTRO_VERSION       = "4.9.88-2.0.0"
TUNE_FEATURES        = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU           = "hard"
meta                 
meta-poky            = "HEAD:0ec241873367e18f5371a3ad9aca1e2801dcd4ee"
meta-oe              
meta-multimedia      = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"
meta-freescale       = "HEAD:49ac225a38f6d84519798e3264f2e4d19b84f70a"
meta-freescale-3rdparty = "HEAD:1d6d5961dbf82624b28bb318b4950a64abc31d12"
meta-freescale-distro = "HEAD:0ec6d7e206705702b5b534611754de0787f92b72"
meta-bsp             
meta-sdk             = "HEAD:d65692ecb3a4136fc1cc137152634e8633ddb3c6"
meta-browser         = "HEAD:d6f9aed41c73b75a97d71bff060b03a66ee087b1"
meta-gnome           
meta-networking      
meta-python          
meta-filesystems     = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"
meta-qt5             = "HEAD:32bb7d18a08d1c48873d7ab6332d4cc3815a4dff"

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:36
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: assimp-4.0.0-r0 do_compile: Function failed: do_compile (log file is located at /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/temp/log.do_compile.55433)
ERROR: Logfile of failure stored in: /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/temp/log.do_compile.55433
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: VERBOSE=1 cmake --build /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build -- -j 1
| /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot-native/usr/bin/cmake -H/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git -B/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build --check-build-system CMakeFiles/Makefile.cmake 0
| /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot-native/usr/bin/cmake -E cmake_progress_start /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/CMakeFiles /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/CMakeFiles/progress.marks
| make -f CMakeFiles/Makefile2 all
| make[1]: Entering directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| make -f contrib/irrXML/CMakeFiles/IrrXML.dir/build.make contrib/irrXML/CMakeFiles/IrrXML.dir/depend
| make[2]: Entering directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| cd /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build && /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot-native/usr/bin/cmake -E cmake_depends "Unix Makefiles" /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/contrib/irrXML /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/contrib/irrXML /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/contrib/irrXML/CMakeFiles/IrrXML.dir/DependInfo.cmake --color=
| make[2]: Leaving directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| make -f contrib/irrXML/CMakeFiles/IrrXML.dir/build.make contrib/irrXML/CMakeFiles/IrrXML.dir/build
| make[2]: Entering directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| make[2]: Nothing to be done for 'contrib/irrXML/CMakeFiles/IrrXML.dir/build'.
| make[2]: Leaving directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| [  1%] Built target IrrXML
| make -f code/CMakeFiles/assimp.dir/build.make code/CMakeFiles/assimp.dir/depend
| make[2]: Entering directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| cd /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build && /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot-native/usr/bin/cmake -E cmake_depends "Unix Makefiles" /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/code /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/code/CMakeFiles/assimp.dir/DependInfo.cmake --color=
| make[2]: Leaving directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| make -f code/CMakeFiles/assimp.dir/build.make code/CMakeFiles/assimp.dir/build
| make[2]: Entering directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| [  1%] Building CXX object code/CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o
| cd /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/code && /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++  -DASSIMP_BUILD_DLL_EXPORT -DASSIMP_BUILD_NO_C4D_IMPORTER -DASSIMP_BUILD_NO_OWN_ZLIB -DASSIMP_IMPORTER_GLTF_USE_OPEN3DGC=1 -DOPENDDLPARSER_BUILD -DOPENDDL_NO_USE_CPP11 -D_FILE_OFFSET_BITS=64 -Dassimp_EXPORTS -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/. -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build/include -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/include -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot/usr/include -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code/../contrib/rapidjson/include -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code/../contrib -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code/../contrib/unzip -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/contrib/irrXML -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code/../contrib/openddlparser/include -I/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code/..  -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9  --sysroot=/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot  -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0=/usr/src/debug/assimp/4.0.0-r0 -fdebug-prefix-map=/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot=  -fvisibility-inlines-hidden  -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9  --sysroot=/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/recipe-sysroot -fopenmp -g -fvisibility=hidden -fPIC -Wall -std=c++0x -fPIC   -o CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o -c /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/git/code/IFCReaderGen1.cpp
| arm-poky-linux-gnueabi-g++: internal compiler error: Killed (program cc1plus)
| Please submit a full bug report,
| with preprocessed source if appropriate.
| See <https://gcc.gnu.org/bugs/> for instructions.
| code/CMakeFiles/assimp.dir/build.make:2849: recipe for target 'code/CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o' failed
| make[2]: *** [code/CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o] Error 4
| make[2]: *** Deleting file 'code/CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o'
| make[2]: Leaving directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| CMakeFiles/Makefile2:193: recipe for target 'code/CMakeFiles/assimp.dir/all' failed
| make[1]: *** [code/CMakeFiles/assimp.dir/all] Error 2
| make[1]: Leaving directory '/home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'
| Makefile:132: recipe for target 'all' failed
| make: *** [all] Error 2
| WARNING: exit code 2 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/okado/imx-yocto-bsp/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/temp/log.do_compile.55433)
ERROR: Task (/home/okado/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.0.0.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3634 tasks of which 3633 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/okado/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.0.0.bb:do_compile
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ラベル(3)
4 返答(返信)

2,940件の閲覧回数
mattnnz
Contributor I

If anyone else meets this issue, try increasing the memory available to your VM or Docker container or run on a machine with more memory. I set my docker container to have 4GB available and this exact problem stopped occurring. This is a common problem on yocto when you get a task terminating without any sort of definitive error.

0 件の賞賛
返信

2,939件の閲覧回数
heqian
Contributor I

I had the same issue with:

  • A clean Ubuntu 14.04
  • Exactly followed "i.MX_Yocto_Project_User's_Guide_Linux.pdf" (Document Number: IMXLXYOCTOUG, Rev. L4.9.88_2.0.0-ga, 05/2018)
  • No change to the .conf files

Error information:

| make[2]: *** [code/CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o] Error 4

| make[2]: *** Deleting file `code/CMakeFiles/assimp.dir/IFCReaderGen1.cpp.o'

| make[2]: *** Waiting for unfinished jobs....

| make[2]: Leaving directory `/root/imx-yocto-bsp/test_proj/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'

| make[1]: *** [code/CMakeFiles/assimp.dir/all] Error 2

| make[1]: Leaving directory `/root/imx-yocto-bsp/test_proj/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/build'

| make: *** [all] Error 2

| WARNING: exit code 2 from a shell command.

| ERROR: Function failed: do_compile (log file is located at /root/imx-yocto-bsp/test_proj/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.0.0-r0/temp/log.do_compile.99434)

ERROR: Task (/root/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.0.0.bb:do_compile) failed with exit code '1'

0 件の賞賛
返信

2,940件の閲覧回数
okado-tomohiro
Contributor I

Hello gusarambula,

Thank you for your responce.

I have not changed the recipie and  local.conf file,just trying according to the "i.MX_Yocto_Project_User's_Guide".

Regards,

0 件の賞賛
返信

2,940件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tomohito Okado,

Have you changed anything on the recipie or local.conf file?

Looks like it’s only the assimp recipe that is failing. I will try to reproduce the error but in an Ubuntu 14.04 machine, which is the recommended host OS. I will let you know as soon as I have more information.

Regards,

0 件の賞賛
返信