Hello,
I get this error, when i try to compile the Android Q10.0.0_2.3.0 (Linux 5.4 kernel)
I use:
Documentation
[ 67% 74832/110113] //system/core/fastboot:libfastboot clang++ socket.cpp [linux_glibc]
[ 67% 74833/110113] //external/setupcompat:setupcompat resource file list [common]
[ 67% 74834/110113] //system/core/fastboot:libfastboot clang++ fs.cpp [linux_glibc]
[ 67% 74835/110113] //frameworks/rs:rs_generated_headers generate
[ 67% 74836/110113] //external/setupdesign:setupdesign-strings aapt2 compile external/setupdesign/strings/res [common]
[ 67% 74837/110113] test android/soong/symbol_inject
[ 67% 74838/110113] //external/setupdesign:setupdesign-strings resource file list [common]
[ 67% 74839/110113] //system/core/fastboot:libfastboot clang++ udp.cpp [linux_glibc]
[ 67% 74840/110113] test host_bionic_inject
[ 67% 74841/110113] //frameworks/rs:rs_generated_sources generate
[ 67% 74842/110113] test android/soong/ui/build/paths
FAILED: out/soong/.bootstrap/soong-ui-build-paths/test/test.passed
out/soong/.bootstrap/bin/gotestrunner -p ./build/soong/ui/build/paths -f out/soong/.bootstrap/soong-ui-build-paths/test/test.passed -- out/soong/.bootstrap/soong-ui-build-paths/test/test -test.short
--- FAIL: TestSendLog (0.00s)
--- FAIL: TestSendLog/Long_name (0.00s)
logs_test.go:43: mkdir /home/user03/android_build/out/soong/.temp/ssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssss916112897: file name too long
--- FAIL: TestSendLog/Long_name_proc_fallback (0.00s)
logs_test.go:43: mkdir /home/user03/android_build/out/soong/.temp/ssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssss889577324: file name too long
--- FAIL: TestSendLog/Long_name_tmp_fallback (0.00s)
logs_test.go:43: mkdir /home/user03/android_build/out/soong/.temp/ssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssssss208601563: file name too long
FAIL
[ 67% 74843/110113] cp out/soong/host/linux-x86/bin/host_bionic_inject
[ 67% 74844/110113] //external/setupdesign:setupdesign aapt2 compile external/setupdesign/main/res 2 [common]
[ 67% 74845/110113] //external/mksh:sh link sh
[ 67% 74846/110113] //system/core/fastboot:libfastboot clang++ usb_linux.cpp [linux_glibc]
[ 67% 74847/110113] //external/setupdesign:setupdesign aapt2 compile external/setupdesign/main/res [common]
[ 67% 74848/110113] //tools/dexter/slicer:slicer link slicer.so [linux_glibc]
[ 67% 74849/110113] //system/core/adb:libadbd_core clang++ daemon/usb_legacy.cpp
[ 67% 74850/110113] out/soong/host/linux-x86/bin/manifest-merger --main out/soong/.intermediates/external/setupdesign/setupdesign/android_common/manifest_fixer/AndroidManifest.xml --libs out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.core_core/android_common/manifest_merger/AndroidManifest.xml --libs out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.legacy_legacy-support-core-ui/android_common/manifest_merger/AndroidManifest.xml --libs out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.appcompat_appcompat/android_common/manifest_merger/AndroidManifest.xml --libs out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.recyclerview_recyclerview/android_common/manifest_merger/AndroidManifest.xml --libs out/soong/.intermediates/external/setupcompat/setupcompat/android_common/manifest_fixer/AndroidManifest.xml --libs out/soong/.intermediates/external/setupdesign/setupdesign-strings/android_common/manifest_fixer/AndroidManifest.xml --out out/soong/.intermediates/external/setupdesign/setupdesign/android_common/manifest_merger/AndroidManifest.xml
[ 67% 74851/110113] link out/soong/.bootstrap/soong-ui-logger/test/test
[ 67% 74852/110113] //frameworks/rs:libRS_internal clang++ rsApiAllocation.cpp
[ 67% 74853/110113] //system/core/adb:libadbd_core clang++ transport.cpp
[ 67% 74854/110113] //bootable/recovery:recovery link recovery
[ 67% 74855/110113] //system/core/adb:libadbd_core clang++ daemon/usb.cpp
[ 67% 74856/110113] //system/core/fastboot:libfastboot clang++ fastboot_driver.cpp [linux_glibc]
[ 67% 74857/110113] //system/core/fastboot:libfastboot clang++ fastboot.cpp [linux_glibc]
ninja: build stopped: subcommand failed.
14:37:11 ninja failed with: exit status 1
[0;31m#### failed to build some targets (01:44:18 (hh:mm:ss)) ####[00m
_ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _
OS: Ubuntu 16.04
it looks:
uboot -> Ok
Kernel -> OK
Android Build -> Fail
i try to re-compile, after make clean & make clobber, but no results!
Best regards
Hello,
Got it, it is to discard hardware issues, but this now seems that the building machine is running out resources for which it will be helpful to check that, especially if it is a virtual machine.
BR,
Ivan.
Hello,
Processor: i.MX 8MQuad and as Board "the i.MX 8MQuad Evaluation Kit (EVK)"
Thanks for you support.
Ruben
Hello,
could you please provide information about the i.MX processor and if it is an evaluation board or a custom one?
Thank you.
BR,
Ivan.