Hi,
I have a requirement to setup inter-processor communication between A53 and M4 using Messaging Unit. I know there is RPMsg available but the requirement demands IPC realization directly on MU.
Is it possible to realize IPC directly on MU?
And if yes, please share the procedure and test application for the same.
The SoC I am working on is IMX8M MINI and Yocto Dunfell.
Regards,
Bhargava
Seamless communication between Cortex-A53 and Cortex-M4 is essential for efficient embedded system operation. NXP’s Messaging Unit (MU) and the RPMsg protocol enable reliable data exchange and coordination between these heterogeneous cores. Proper implementation ensures smooth inter-processor messaging for real-time applications.
Bump!
I know it's 4 years later, but still, bump.
I'm on a i.MX8MP, so I have a M7 in baremetal and the 4x A53 cores running Linux. In the baremetal I can use:
Hello,
I needed one information. Do you have mcmgr in your SDK which you downloaded from NXP site?
Hi,
Thanks for replying.
Actually I am referring to Asymmetric Multiprocessing between Cortex-A53 and Cortex-M4.
Instead of using RPMsg (Remote Processor Messaging) for the same, is there a possibility to realize inter-processor communication directly on Messaging Unit(MU)?
Are these APIs [sc_ipc_open() , sc_ipc_read(), sc_ipc_write(), sc_ipc_close()] available in the linux mainline, Because I could not find any of them in the entire kernel source.
Please provide information about how those APIs can be used along with an user space application(if any).
Regards,
Bhargava