Color issues capturing analog video with TVP5147 and i.MX51

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Color issues capturing analog video with TVP5147 and i.MX51

2,045件の閲覧回数
LautaroCarmona1
Contributor II

About our colour issues while capturing:

We are working with BlueTechnix SBC-i.MX51 and Texas Instrument TVP5147 Video Decoder.

After loading the corresponding modules:

modprobe tvp5147_tvin

modprobe mxc_v4l2_capture

 

We tried the following in order to capture raw video:

cd /unit_tests/

./mxc_v4l2_capture.out -ih 680 -iw 240 -oh 640 -ow 360 -fr 30 -f YUYV test.yuv

 

We were able to do it, and then we could play it with mplayer on our host machine with: "mplayer -rawvideo w=640:h=360:fps=30:f=YUY2 -demuxer rawvideo" 

 

While doing this we found some color issues.

With this post I'm uploading a picture where this can be appreciated (we use the plain colors Blue, Red and Green as inputs, and a TestSignal too).

As it can be seen, the colour is well displayed only at certain alternating vertical bars.

Any ideas of what may the problem is?

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,910件の閲覧回数
LautaroCarmona1
Contributor II

Hi Hake,

We found that the problem was being caused by a hardware issue of our tvp5147 tvin board.

We asked Texas Instrument people, and we found out that we had a bad crystal on our board, here is the forum where we discussed it:

http://e2e.ti.com/support/data_converters/videoconverters/f/376/p/142207/513278.aspx#513278

Thanks for your interest!

Regards,

Lautaro.

0 件の賞賛
返信

1,910件の閲覧回数
hake
NXP Employee
NXP Employee
can you use ./mxc_v4l2_capture.out -ih 680 -iw 240 -oh 640 -ow 360 to output the screen and see the result? if the problem exist in display, I guess the input signal need some fine tune for tvp5147_tvin.
0 件の賞賛
返信