Coin cell charge current in PF3000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coin cell charge current in PF3000

Jump to solution
840 Views
ko-hey
Senior Contributor II

Hi all

Considering that the coin type battery will be charged, we would like to calculate the battery life.

Please give me the maximum value of the current flowing from the PMIC to the coin type battery while the voltage is being supplied to VIN.

According to the table 29 of PF3000.pdf, typical value of coin cell charge current is 60uA and  accuracy is ±30%.

So I think the value of max and min is as follow.

Max: 78uA

Typ: 60uA

Min: 42uA

Are the above coin cell charge current values correct ?

 

Ko-hey

Labels (3)
0 Kudos
Reply
1 Solution
696 Views
art
NXP Employee
NXP Employee

Yes, the maximum charge current to fully discharged coin cell battery of the PF3000 PMIC is in range of 42uA to 78uA.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
697 Views
art
NXP Employee
NXP Employee

Yes, the maximum charge current to fully discharged coin cell battery of the PF3000 PMIC is in range of 42uA to 78uA.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply