Cloning several DTB files to another SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cloning several DTB files to another SD card

697 Views
BufferGHz
Contributor I

I have each of the individual files, do I need to build them together into the u-boot.bin file?  If so, what software can be used? One of the files is a uimage file which is Linux.  I have tried simply copying the files and reformatting an SD card but this is still not working. 

0 Kudos
Reply
2 Replies

682 Views
BufferGHz
Contributor I

@Bio_TICFSL Thanks. Can you provide information on doing so? I assume it needs to be complied.  

0 Kudos
Reply

688 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello BufferGHz,

You need to build all together with make dtb in your kernel. if your SD doesnt work could be that the dtb is not working correctly, or other fail.

 

regards

 

0 Kudos
Reply