Cloning rootfs partition of emmc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cloning rootfs partition of emmc

1,485件の閲覧回数
pratyushtomar
Contributor IV

I have a customised board based on imx6ul evk. We are using emmc on this board. So we are using one board for testing and after completing it's testing we want to clone the yocto image on this board and use this same image in other boards. Is their any way to clone the image?

ラベル(3)
0 件の賞賛
返信
1 返信

1,346件の閲覧回数
art
NXP Employee
NXP Employee

For the information on how to prepare a boot media (including eMMC) for the i.MX6 series processors, please refer to the Chapter 4 "Booting Linux OS" of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信