Cloning rootfs partition of emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cloning rootfs partition of emmc

1,541 Views
pratyushtomar
Contributor IV

I have a customised board based on imx6ul evk. We are using emmc on this board. So we are using one board for testing and after completing it's testing we want to clone the yocto image on this board and use this same image in other boards. Is their any way to clone the image?

Labels (3)
0 Kudos
Reply
1 Reply

1,402 Views
art
NXP Employee
NXP Employee

For the information on how to prepare a boot media (including eMMC) for the i.MX6 series processors, please refer to the Chapter 4 "Booting Linux OS" of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply