Dear all,
I see the following chapter of the reference manual.
i.MX 6UltraLite i.MX 6UltraLite (Rev.1)
- 22.4 Clocks (P.879)
"The table found here describes the clock sources for ENET. Please see for clock setting, configuration and gating information."
I cannot find Table.
Would you send Table?
I understand that Clock source for ENET is PLL6.
Can I choose PLL2 as Clock source for ENET?
Best Regards,
Yuuki
Solved! Go to Solution.
Actually, this is just a confusing statement in the manual. Only PLL6 can be used as the clock source for the ENET module. For the information on PLL6 configuration and clock gating, refer to the Chapter 18 "Clock Controller Module (CCM)" of the Reference Manual document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Actually, this is just a confusing statement in the manual. Only PLL6 can be used as the clock source for the ENET module. For the information on PLL6 configuration and clock gating, refer to the Chapter 18 "Clock Controller Module (CCM)" of the Reference Manual document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------