Clarification of the Hardware Checklist i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clarification of the Hardware Checklist i.MX6

ソリューションへジャンプ
1,663件の閲覧回数
bomsweigh
Contributor I

Hello,

We are finishing up the design of an IMX6 and we had a question about the three lines below.  They come from the hardware design checklist. The questions are:

12a. What does a tandem 0Ohm resistor mean?  Tandem to what?

12b Is the SD port clock trace the same as SDx_CLK?

13 From our reading of the errata/apnote, the safest method to accomplish this is to provide an external circuit to power down the SD cards?

14 Do we understand correctly that an in-line zero Ohm resistor is required on all of the SDx_CLK lines between the i.MX and the SD Card?

Thank you for the guidance,

BW

     

Not Sure12Add reserved tandem 0Ω resister in SD port clock trace and place near i.Mx6 side for SI consideration. CUS
Not Sure13Please keep i.Mx6 "SDx_RESET" pin connecting properly with device reset pin  when eMMC/SD fast boot is used in a design. (i.M6DQ AC and i.MX6SDL AB version had fixed this issue, don't need consider this item.) See below need to add I/O line to cycle SD card power.
Not Sure14NAND_RE and SDx_CLK are loop back as internal reference clock at internal  pad, recommend adding a series 0hom resister on these two signals and place near i.Mx6 pin side to reduce the potential reflect SI issue.” CUS
ラベル(1)
0 件の賞賛
返信
1 解決策
1,498件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Boms

12a. 0Ohm resistor is used for testing and bringup purposes, can be removed in final design. 

12b yes

13 usage of SD card "Reset" signal is described in SD specifications.

14 zero Ohm resistor is not required

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,499件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Boms

12a. 0Ohm resistor is used for testing and bringup purposes, can be removed in final design. 

12b yes

13 usage of SD card "Reset" signal is described in SD specifications.

14 zero Ohm resistor is not required

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,498件の閲覧回数
bomsweigh
Contributor I

Thank you very much.

0 件の賞賛
返信