Clarification for i.MX6 Dual/Quad Datasheets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clarification for i.MX6 Dual/Quad Datasheets

Jump to solution
855 Views
MOW
Contributor IV

Hi all

All Rev.4 Datasheets from 07/2015 for the i.MX6 Dual/Quad SoCs list in chapter "7 Revision History" the point "Table 6, "Operating Ranges," on page 21: Changed value: Standby/DSM Mode, VDD_SOC_IN, minimum voltage, from 0.9V to 1.05V." but in all Rev.4 Datasheets Table 6 on page 21 still lists "Standby/DSM mode VDD_SOC_IN" as minimum of 0.9V.

Which one is the correct minimum voltage: the 0.9V still listed in table 6 on page 21, or the claimed (but apparently not really made) change to 1.05V mentioned in the Rev.4 Change History?

Kind Regards,

Marc

Labels (2)
0 Kudos
1 Solution
685 Views
Yuri
NXP Employee
NXP Employee

Hello,

"The datasheet values should have been changed to 1.05V

(per the revision history entry). That will be corrected in the
next revision."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
685 Views
MOW
Contributor IV

Hi Yuri

Thanks for the clarification. Is such a change also necessary for the i.MX6 Solo/DualLite SoCs? The most recent datasheets for these don't mention any changes to VDD_SOC_IN, at all, so far.

Kind regards,

Marc

0 Kudos
685 Views
Yuri
NXP Employee
NXP Employee

Hi,

  The needed changes will be provided for other devices of i.MX6 series, but please

use the current releases as is now. I meant  the i.MX6 Solo/DualLite SoCs.

Regards,

Yuri.

0 Kudos
686 Views
Yuri
NXP Employee
NXP Employee

Hello,

"The datasheet values should have been changed to 1.05V

(per the revision history entry). That will be corrected in the
next revision."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos