Chromium48 hangs up when rendering a new page in a tab

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chromium48 hangs up when rendering a new page in a tab

1,276 Views
wangjunqiang
Contributor I

Hi,all:

      I built the yocto(fsl-release-bsp) images(fsl-image-x11) with the Chromium browser integrated into it.

When I use a browser to open a page in the new tab, the browser will crash.

But,When I use a browser to open a page in the new window,the browser is OK. It is also ok to open a blank tab.

And if I do not check "use hardware acceleration when available" ,everything is good.

When the browser crashes, glmark2 can not run.

Similar to my question:

https://www.mail-archive.com/openembedded-devel@lists.openembedded.org/msg50205.html 

i.MX6 DL, Yocto Krogoth and Chromium 48.0.2548 problems ... 

How can i solve this problem?

What should I do to make the browser work stably using the GPU?

 

Thanks

Labels (4)
0 Kudos
Reply
1 Reply

1,026 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi wang,

Several issues and bugs are reported for Chromium on latest yocto bsp New chromium version works only on X11 and VPU patches do not apply on new version. For Wayland use older chromium version renamed to chromium-wayland and add VPU patches, Chromium in the older BSP versions were more stable, but they aren't patched for GCC5.

hope this helps