Chromium on imx-6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Chromium on imx-6

1,463 次查看
buddhikedesilva
Contributor II

I've created sato image with chromium using fsl-community-bsp. However, when I launch it from desktop, the device reboots.

GitHub - Freescale/chromium-imx​ mentions that you have to use --use-gl=egl. I'm not sure if the desktop link is providing this.

Should this cause the device to reboot if this was the case though?

I'm thinking, if I build x11 image should I be able to run chromium with this option. Has anyone else been able do this before?

0 项奖励
回复
1 回复

994 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  You may try NXP BSP - please refer to section 5.6.6 (Chromium Browser on X11,
XWayland and Wayland) of "Freescale_Yocto_Project_User's_Guide.pdf".

https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&location=null&fpsp=1&WT_TYPE=S...

 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复