Hello All,
We are tying to run chromium on Wayland Weston compositor.
I am using YOCTO linux distribution in i.MX6Q Sabre SD board.
Chromium version = 48.0.25
Kernel version = 4.1.28-fslc+g0844f
Weston Version = 1.9.0
EGL version = 1.4
Used following command to run on Weston terminal.
> google-chrome
Getting following error
[534:534:0725/083535:ERROR:desktop_window_tree_host_ozone.cc(572)] Not implemented reached in virtual void view
s::DesktopWindowTreeHostOzone::SetWindowIcons(const gfx::ImageSkia&, const gfx::ImageSkia&)
[534:534:0725/083535:ERROR:ozone_webui.cc(60)] Not implemented reached in virtual void views::OzoneWebUI::GetDe
faultFontDescription(std::__cxx11::string*, int*, int*, gfx::FontRenderParams*) const
[534:534:0725/083535:ERROR:ozone_webui.cc(51)] Not implemented reached in virtual gfx::FontRenderParams views::
OzoneWebUI::GetDefaultFontRenderParams() const
[534:534:0725/083535:ERROR:ozone_webui.cc(51)] Not implemented reached in virtual gfx::FontRenderParams views::
OzoneWebUI::GetDefaultFontRenderParams() const
[534:534:0725/083535:ERROR:ozone_webui.cc(51)] Not implemented reached in virtual gfx::FontRenderParams views::
OzoneWebUI::GetDefaultFontRenderParams() const
[534:534:0725/083535:ERROR:ozone_webui.cc(51)] Not implemented reached in virtual gfx::FontRenderParams views::
OzoneWebUI::GetDefaultFontRenderParams() const
[534:534:0725/083535:ERROR:ozone_webui.cc(51)] Not implemented reached in virtual gfx::FontRenderParams views::
OzoneWebUI::GetDefaultFontRenderParams() const
[562:562:0725/083535:ERROR:sandbox_linux.cc(338)] InitializeSandbox() called with multiple threads in process g
pu-process
[534:534:0725/083535:ERROR:ozone_webui.cc(51)] Not implemented reached in virtual gfx::FontRenderParams views::
OzoneWebUI::GetDefaultFontRenderParams() const
/usr/bin/google-chrome: line 11: 534 Segmentation fault /usr/bin/chromium/chrome ${CHROME_EXTRA_ARGS} $@
Please help me to resolve this issue.
Thanks,
Senthil.
Hi All,
I have the similar problem with the same version of chromium, but with the following system:
Device : imx6qdl (custom board, based on SabreSD)
Kernel version = 3.14.52+g5f6f0a5
Weston Version = 1.9.0
imx-gpu-viv = 5.0.11.p7.4
Terminal output:
root@imx6qh120:~# /usr/bin/chromium/chrome --use-gl=egl --user-data-dir=/home/chrome
[2702:2702:0922/105852:FATAL:browser_main_loop.cc(202)] Running without the SUID sandbox! See https://code.google.com/p/chromium/wiki/LinuxSUIDSandboxDevelopment for more information on devel.
#0 0x00007319780a <unknown>
#1 0x0000731a6f8e <unknown>
#2 0x000074bbd210 <unknown>
#3 0x000074a69bd4 <unknown>
#4 0x000074a690b0 <unknown>
#5 0x000073168ef0 <unknown>
#6 0x00007316874a <unknown>
#7 0x000072e97b5c ChromeMain
#8 0x00007207bcf8 __libc_start_mainAborted
If someone got Chromium 48 working on a linux-imx kernel and weston 1.9.0, I am interested in knowing about the kernel+imc-gpu-viv config, as well as the chromium launch command involved.
Thanks,
Thomas
Hi Senthil
one can try with nxp bsp and please refer to attached Yocto Guide
sect.5.6.6 Chromium Browser on X11 and Wayland
i.MX 6 Series Software and Development Tool|NXP
regarding l4.1.28-fslc one can post on meta-fsl-arm mailing list,
so that someone familiar with that version could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
community (fslc) vs nxp official bsp :
https://community.freescale.com/message/402940#402940
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------