Chromium Issue with i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chromium Issue with i.MX8

1,881 Views
thom
Contributor II

Hay, 

i build the i.MX8MM bep fsl-validation-image-imx for the 8MM with Chromium. But i get every time the same fail if i try to start

sh-4.4# chromium --no-sandbox --
EGL: Warning: No default display support on wayland
[4377:4377:0312/141334.717889:ERROR:gl_surface_egl.cc(935)] EGL display query failed with error EGL_SUCCESS
[4377:4377:0312/141334.717940:ERROR:gl_surface_egl.cc(949)] eglInitialize Default failed with error EGL_BAD_DISPLAY
[4377:4377:0312/141334.717968:ERROR:gl_ozone_egl.cc(20)] GLSurfaceEGL::InitializeOneOff failed.
[4377:4377:0312/141334.722679:ERROR:viz_main_impl.cc(184)] Exiting GPU process due to errors during initialization
[4349:4382:0312/141334.747410:ERROR:bus.cc(396)] Failed to connect to the bus: Could not parse server address: Unknown address type (examples of valid types are
"tcp" and on UNIX "unix")
[4349:4349:0312/141334.782730:ERROR:desktop_window_tree_host_platform.cc(441)] Not implemented reached in virtual void views::DesktopWindowTreeHostPlatform::Init
ModalType(ui::ModalType)
[4349:4349:0312/141334.782864:ERROR:desktop_window_tree_host_platform.cc(451)] Not implemented reached in virtual bool views::DesktopWindowTreeHostPlatform::IsAn
imatingClosed() const
[4349:4349:0312/141334.784728:ERROR:desktop_window_tree_host_platform.cc(464)] Not implemented reached in virtual void views::DesktopWindowTreeHostPlatform::Size
ConstraintsChanged()
[4349:4349:0312/141334.813750:ERROR:desktop_window_tree_host_platform.cc(435)] Not implemented reached in virtual void views::DesktopWindowTreeHostPlatform::SetW
indowIcons(const gfx::ImageSkia&, const gfx::ImageSkia&)
[4349:4349:0312/141334.813897:ERROR:desktop_window_tree_host_platform.cc(373)] Not implemented reached in virtual bool views::DesktopWindowTreeHostPlatform::SetW
indowTitle(const string16&)
[4349:4349:0312/141334.856276:ERROR:desktop_window_tree_host_platform.cc(311)] Not implemented reached in virtual void views::DesktopWindowTreeHostPlatform::Acti
vate()
[4349:4349:0312/141334.859841:ERROR:desktop_window_tree_host_platform.cc(222)] Not implemented reached in virtual bool views::DesktopWindowTreeHostPlatform::IsVi
sible() const
[4349:4349:0312/141334.916910:ERROR:wayland_connection_connector.cc(48)] Not implemented reached in virtual void ui::WaylandConnectionConnector::OnChannelDestroy
ed(int)
Segmentation fault (core dumped)

0 Kudos
2 Replies

1,427 Views
cphealy1
Senior Contributor I

If you want to run with Wayland/Weston, you might want to try WPE (Webkit Port for Embedded).  It works with Wayland/Weston.  If you try WPE, please make sure to run the latest version that was released several weeks ago as a good amount of work was done to optimize Wayland performance.

WPE WebKit 

WPE | WebKit 

0 Kudos

1,427 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Thomas,

There is no support of Chromium on Wayland.

0 Kudos