Choosing where to run inference from application code - GPU/NPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Choosing where to run inference from application code - GPU/NPU

Jump to solution
710 Views
StefanoN
Contributor I

Hello.

Normally inference is run on the GPU or NPU based on the USE_GPU_INFERENCE=0/1 env. variable, but I would like to make this choice in code. In the Machine Learning guide it says that that variable is "directly read by the HW acceleration driver".

StefanoN_0-1743595701752.png

Is it feasible to modify the GPU/NPU unified driver to expose this functionality to high abstraction layers? Where can I find it?

If not, What else could I do?

Thanks

 

 

0 Kudos
Reply
1 Solution
661 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @StefanoN!

 

The source code is not public yet, even for us due to the GPU is not an NXP IP, our vendor provides the compiled binary for us.

View solution in original post

4 Replies
683 Views
StefanoN
Contributor I

I understand. Nonetheless can you help me locate the code for the unified driver?

0 Kudos
Reply
697 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @StefanoN!

Thank you for contacting NXP Support!

 

Unfortunately there is no way to do it different that we mentioned in our MACHINE LEARNING USER GUIDE.

 

Best Regards!

Chavira

0 Kudos
Reply
667 Views
StefanoN
Contributor I

My understanding is that the so called NPU/GPU driver is found in the Yocto directory `meta-freescale/recipes-graphics/imx-gpu-viv`, but the SRC_URI is given as `${FSL_MIRROR}/${BPN}-${PV}-${IMX_SRCREV_ABBREV}.bin` which at runtime resolves to `https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.11.p2.6-aarch64-bc7b6a2.bin`.

Looking in the forum I found this user asking for the source code (https://community.nxp.com/t5/i-MX-Processors/GPU-source-code-with-opencl/m-p/1224323)

It was not public in 2021, is it still not public now?

 

Thanks

0 Kudos
Reply
662 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @StefanoN!

 

The source code is not public yet, even for us due to the GPU is not an NXP IP, our vendor provides the compiled binary for us.