Choosing 24MHz Crystal Oscillator for i.MX535

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Choosing 24MHz Crystal Oscillator for i.MX535

863件の閲覧回数
neeveehariharan
Contributor I

Hi,

What should be the Load capacitance of the 24MHz crystal oscillator?

The i.MX53 user manual (Page 32) states that, the crystal must be rated for a maximum drive level of 100 μW or higher and an ESR of 80 Ω or less is recommended.

The i.MX53 reference manual (chapter 79, crystal oscillator 24MHz), also does not mention about the load capacitance.

Can I get any help on this?

 

Thanks and Regards,

Hari

ラベル(1)
0 件の賞賛
返信
1 返信

735件の閲覧回数
Yogesh1z
Contributor I

Hi,

Please refer to Datasheet (IMXCEC version E) Page of 149. I am pasting textt here.

( Due to XTALOSC automatic level controller, the power consumption depends heavily on the working frequency, C-load and crystal quality. The above results are achieved at a frequency 24 MHz, 10 pF load capacitor, 7 pF crystal shunt capacitor and 80 Ω ESR.)

Yogesh

0 件の賞賛
返信