ello,
first: sorry for my english.
Setup: Mx28 with USB0 connect to linux PC. USB0 is capable of OTG.
USB0 is set up to be an OTG device. I am running linux 3.10 rc6. I would like to turn the USB0 into a gadget_serial device so I can talk to it from the PC using minicom.
I compiled the linux image with the following config:
CONFIG_USB_CHIPIDEA=m
CONFIG_USB_CHIPIDEA_UDC=y
CONFIG_USB_CHIPIDEA_HOST=y
CONFIG_USB_CHIPIDEA_DEBUG=y
CONFIG_USB_GADGET=m
CONFIG_USB_G_SERIAL=m
I can't load the g_serial module because it couldn't find any UDC device. This is the chipidea core did not register any udc device in the udc_device list. The reason: it thinks the USB0 is a host device instead of a gadget device.
I put print statement inside the driver and observed the following:
Inside /chipidea/core.c: ci_hdrc_probe(), after calling ci_hdrc_gadet_init(ci), the result is a dual role for both host and gadget. This is correct since the DCCPARAMS register has both HC and DC bits set to 1. However, afterward, it calls ci_otg_role(ci). The result is always return as HOST. This is because bit OTGSC_ID of the OTGSC register is reporting 0 which stand for A device.
As i understand, and that's not much, the PC and the mx28 negotiate and determine who can be host/device. I would expect that the OTGSC register reports result of this negotiation. When and where does this happen? I also expect that the MX28 will be a Device, where did it go wrong?
What is the appropriate step to turn the USB0 into a gadget device?
What do I need as far as device tree? configuration?
Or is there a bug somewhere that cause the device to always be a host?
what am i missing?
Gosh, i am desperate.
Here is a catch: with the same hardware setup and the mx28 running kernel 2.6, works like a charm.
I appreciate any idea.
here is the device tree for USB0
usb0: usb@80080000 {
vbus-supply = <®_usb0_vbus>;
disable-over-current;
status = "okay";
};
reg_usb0_vbus: usb0_vbus {
compatible = "regulator-fixed";
regulator-name = "usb0_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
enable-active-high;
};