Changing available memory on Nitrogen6x board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing available memory on Nitrogen6x board

1,708件の閲覧回数
yt
Contributor I

I am using nitrogen6x Solo board with 1GB DDR3 RAM with 3.0.35 kernel.

I wanted to try to limit the available memory to 128 MB. I have tried to change the DDR_MB size on the boards.cfg in U-Boot with no luck.

Can someone point me the proper step to do this?

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

1,527件の閲覧回数
EricNelson
Senior Contributor II

Hi Yuldi,

You can add "mem=128M" to the kernel command-line by editing the boot script (6x_bootscript.txt).

The on-line boot script compiler can convert back to the binary form:

          http://git.boundarydevices.com/bootscript.php

Regards,

Eric

1,527件の閲覧回数
yt
Contributor I

Thanks Eric.

Actually the issue was the reserved memory for the GPU was more than the memory size. I reduced the size and I was able to boot just fine.

After the boot I noticed that there is still 16900k reserved, as follows:

Memory: 120MB = 120MB total

Memory: 114172k/114172k available, 16900k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    ...

May I know what other configurations to adjust the kernel reserved memory?

0 件の賞賛
返信

1,527件の閲覧回数
EricNelson
Senior Contributor II

Hi Yuldi,

This isn't information that I have readily available, but in 3.0.35, you can check through the board startup file:

linux-imx6/board-mx6_nit6xlite.c at boundary-imx_3.0.35_4.1.0 · boundarydevices/linux-imx6 · GitHub

0 件の賞賛
返信

1,527件の閲覧回数
EricNelson
Senior Contributor II

Sorry. I thought you said Nitrogen6_Lite.

The corresponding Nitrogen6x solo code is here:

     linux-imx6/board-mx6_nitrogen6x.c at boundary-imx_3.0.35_4.1.0 · boundarydevices/linux-imx6 · GitHub

0 件の賞賛
返信