Changing UART1 to UART3 for u-boot in i.MX7D-SABRE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing UART1 to UART3 for u-boot in i.MX7D-SABRE

428 Views
vijayhs
Contributor I

Hi,

I have a custom board based on i.MX7D-SABRE. I want to change the u-boot console prints from UART1 to UART3. Where all u-boot source code changes to be done for this?

Thanks & Regards

Vijay H.S

Labels (1)
0 Kudos
1 Reply

318 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Vijay,

the following document will be useul. It explains how to migrate U-boot for a custom board which in this case it is Udoo Quad board.

U-Boot Migration Example 


Best regards,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos