Change the size of the image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change the size of the image

384 Views
santhosha
Contributor II

I am using IMX6 bsp with 14.04 supported on Ubuntu to build the image.  I need more control on the image structure to fit different size partitions.  How it can be done?

Also i would like to load the image in different orders such as

image 1 with few drivers will load first, then image 1 starts executing, and image1 loads the image2 and so on.

Is this possible?

Where can i change and control the contents of image that goes to multiple partitions?

My target has emmc as permenant storage.

Please answer.

Labels (1)
0 Kudos
1 Reply

314 Views
b36401
NXP Employee
NXP Employee

You can build several images that use separate partitions of flash and chose one in u-boot.

However we have no such examples. Sorry for the inconvenience.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos