Change the GPIO default level after the board is powered on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change the GPIO default level after the board is powered on

563 Views
Keanight
Contributor I

Hi there,

The SD2_RESET_B(GPIO2_IO19) Pin on i.MX8 mm ekv is reset to high at the very beginning of the booting phase. Is there any way to change this? We want to reuse this pin for another purpose instead of an SD card, and this requires this gpio remain low during the whole booting process.

Thanks

0 Kudos
Reply
0 Replies