Change resolution at runtime on iMX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change resolution at runtime on iMX8

4,505件の閲覧回数
pgentili
Contributor III

Hi everyone,

on our previous system (which was based on imx6dl, yocto krogoth) we were able to support multiple displays for our projects. The displays are connected via LVDS.

Basically we were doing something like this at boot:

  • fbset --timings a b c d e f
  • fbset --geometry a b c d e f
  • /etc/init.d/weston restart

And it worked flawlessy with 3 different displays, with different resolutions.

Now we're trying to implement something similar on imx8mm, yocto sumo. The main difference here is that we are using systemd.

I was expecting to make it work with these steps:

  • fbset --timings a b c d e f
  • fbset --geometry a b c d e f
  • systemctl restart weston

But weston.service is somehow resetting my fbset configuration. This is the message that I get after the service restart:

[ 4724.330511] imx-drm display-subsystem: sn65dsi83_bridge_disable
[ 4724.389148] imx-drm display-subsystem: sn65dsi83_bridge_mode_set: mode: 1280*800@70000
[ 4724.393025] imx-drm display-subsystem: sn65dsi83_bridge_enable
[ 4724.393032] sn65dsi83 3-002c: sn65dsi83_brg_setup
[ 4724.403996] sn65dsi83 3-002c: PIXCLK [ 70000000 ] Hz
[ 4724.404001] sn65dsi83 3-002c: DSI clock [ 420000000 ] Hz
[ 4724.404005] sn65dsi83 3-002c: GeoMetry [ 1280 x 800 ] Hz
[ 4724.408619] sn65dsi83 3-002c: LVDS SINGLE CHANNEL
root@icoremx8mm_alma:~# [ 4725.123157] imx-drm display-subsystem: sn65dsi83_connector_detect
[ 4725.129310] imx-drm display-subsystem: sn65dsi83_connector_get_modes
[ 4725.135728] imx-drm display-subsystem: sn65dsi83_connector_mode_valid: mode: 1280*800@70000 is valid

but the resolution I'm setting with the fbset commands is 1024*798.

I would really not want to write different device trees for each of our diffent product because of maintainability.

Do you have any suggestion to make it work?

Thanks

Paolo Gentili 

タグ(3)
0 件の賞賛
返信
1 返信

4,418件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Paolo,

Use the method, please!

-------------------------------------

1.  To change  output mode to your resolution at "/etc/xdg/weston/weston.ini"

      
[output]
name=HDMI-A-1                       
mode=1920x1080@60

 

2. restart weston 

  systemctl restart weston

--------------------------------------

Have a nice day!

B.R,

weidong