Hi there,
I'm beginner in iMX6. This is several basic question:
S:1920x1080p-60
S:1920x1080p-50
S:1280x720p-60
V:640x480p-60
D:1280x720p-60
V:640x480p-60
1.what is S, D, V, p, i stand for?
2. how can i change resolution of hdmi output?
3. Any example source code for test hdmi. For instance, display something via hdmi?
4. what is difference between "mode" and "modes" in "/sys/class/graphics/fb1/" => done
My system: Linux kernel 3.0.35
dmesg | grep mxc_hdmi
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver hdmi
Thank you,
已解决! 转到解答。
Hi,
tahi
4. what is difference between "mode" and "modes" in "/sys/class/graphics/fb1/"
modes shows the list of supported resolution. and mode provides the information for the current setup resolution.
You change the value in mode from different values of modes.
if xrandr command is available than it can also be used to change the output display.
"xrandr -s 1920x1080" sets output to 1080p
Regards
Saurabh
1.what is S, D, V, p, i stand for?
i: interlaced
p:progressive
Please refer: http://www.serif.com/blog/video-editing-terms-explained-part-2-progressive-p-vs-interlaced-i-recordi...
Hi,
tahi
4. what is difference between "mode" and "modes" in "/sys/class/graphics/fb1/"
modes shows the list of supported resolution. and mode provides the information for the current setup resolution.
You change the value in mode from different values of modes.
if xrandr command is available than it can also be used to change the output display.
"xrandr -s 1920x1080" sets output to 1080p
Regards
Saurabh
Thank you so much.
xrandr return "Can't open display"
What frame buffer (fb0, fb1...) is impacted by "xrandr" ?
In case, i want add more to list of support resolution. How can i do?
Sincerely,
Tahi