Hi, I have used Yocto to create the fsl-image-gui, I'd like to add in a custom script to the RootFS.
I did try adding it into "tmp/work/imx28evk-poky-linux-gnueabi/fsl-image-gui/1.0-r0/rootfs/etc/X11/Xsession.d/" when I rebuild the image using the command "bitbake fsl-image-gui" and copy to SD card the new script doesn't appear.
Can anyone help me please?
已解决! 转到解答。
All custom scripts should be installed from the recipe (.bb file or even better if you create a .bbappend file, into the do_install task). What is the recipe related to this script?. The rootfs to look is the one deploy on tmp/deploy/images/*.tar.bz2. All others rootfs under tmp are used during the build.
Leo
All custom scripts should be installed from the recipe (.bb file or even better if you create a .bbappend file, into the do_install task). What is the recipe related to this script?. The rootfs to look is the one deploy on tmp/deploy/images/*.tar.bz2. All others rootfs under tmp are used during the build.
Leo
If it´s something like xorg.conf, take a look here
https://github.com/Freescale/meta-fsl-arm/tree/master/recipes-graphics/xorg-xserver
if it´s something like rclocal, take a look here:
https://github.com/Freescale/meta-fsl-demos/tree/master/recipes-fsl/fsl-rc-local
Well, it may not be exactly what you want, but I think it may help :smileywink: