Change OV5640 Register Using I2C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change OV5640 Register Using I2C

2,141件の閲覧回数
giritharanr
Contributor I

Hi ,

       I am new to this,please help me to solve my issue,

I want to change some  register values of ov5640.c driver file  from user space c API.

I tried this link( https://www.kernel.org/doc/Documentation/i2c/dev-interface ) .But in this c program i can't change my register value..Here i attach my i2c code.please kindly gothrough it.

 

Thanks in Advance!.

 

 

 

 

 

With REGARDS,

R.Giritharan

Original Attachment has been moved to: i2c_ov5640.c.zip

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,643件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

One suggestion:

You can read the ioctl part in driver source code ov5640.c. You can modify/add one ioctl function and then call that ioctl for changing the register value in user space.

0 件の賞賛
返信

1,642件の閲覧回数
giritharanr
Contributor I

Hi igor,

     Thanks for your reply.

i saw the source code which you attach.

my doubt is , for example i want to change the register 0x5000 value from 0x06 to 0xff from user space...so as per my attached code if i give the reg value of 0x5000 means it won't taken.i don't know why?

so register is not written properly.

please find any solution to over write the register values at run time.

Thanks in advance!

With Regards,

R.Giritharan

0 件の賞賛
返信

1,643件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giritharan

I think it is necessary to use platform specific i2c api as used

for example in unit tests (refer to attached part of it,

I2C Test With mt9v111 camera mxc_i2c_test.c), sources

can be found

http://downloads.yoctoproject.org/mirror/sources/imx-test-5.2.tar.gz

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信