Capturing camera images via the ADV7282-M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capturing camera images via the ADV7282-M

1,563 Views
eishishibusawa
Contributor III

Dear Sir

 

I would like to confirm the driver for ADV7282-M.

Customer is trying to capture the camera image to the i.MX8M(i.MX8M-EVK and L4.9.88_2.0.0) via the ADV7282-M.

 

Q1.

Which driver should we use to capture camera images via the ADV 7282-M?

 

Best Regards,

Eishi SHIBUSAWA

0 Kudos
Reply
2 Replies

1,250 Views
art
NXP Employee
NXP Employee

There is no immediate support for the ADV7282-M video decoder chip in the L4.9.88_2.0.0 Linux BSP on the i.MX8M platform. The customer should use the MIPI-CSI2 port and the corresponding driver, described in the Section 6.1.3 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,250 Views
eishishibusawa
Contributor III

Dear NXP support member

 

Please reply this question.

 

Best Regards,
Eishi SHIBUSAWA

0 Kudos
Reply