Capturing camera frame via user space

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capturing camera frame via user space

2,869 Views
alexandrechartr
Contributor II

Hi,

We car currently trying to integrate an unsupported camera (IMX278) to our custom board built with an IMX6D. The camera uses 4 lanes CSI connection. We use linux kernel 3.14.

What we have done right now is initializing the camera via I2C and generating the pixel clock in user space and everything seems to work fine. Then, I try the unit test mxc_v4l2_capture.out and when I run it I get the following error:

Unable to open /dev/video0
Unable to create y frame recording file

If I run : dmesg | grep v4l

I got this output:

ERROR: v4l2 capture: slave not found!

I have seen that the mxc_v4l2_capture driver only supports some specific cameras. So, here's my questions:

What do I have to modify in the unit test or in the mxc_v4l2 driver to add support for my camera?

Is it possible to do everything in user space or do I need to write a driver?

Is there another way to get the camera frame from user space?

Thank you,

Alexandre

Labels (2)
4 Replies

2,215 Views
mustafabakircio
Contributor IV

Hi alexandrechartrand

Did you solve the capture problem about imx278 ?

0 Kudos
Reply

2,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

next steps could be configuring i.MX6 MIPI phy and checking its MIPI_CSI_PHY_STATE

as described in Debug steps for customer MIPI sensor.docx
https://community.freescale.com/docs/DOC-94312

AN5305 MIPI-CSI2 Peripheral on i.MX6 MPU
http://cache.nxp.com/files/32bit/doc/app_note/AN5305.pdf

what is camera format, one can try to find similar examples on community.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,215 Views
alexandrechartr
Contributor II

Hi Igor,

The camera we use is the imx278 and I haven't found any example that use this camera.

Do I have to use the v4l2 driver to capture frame or is there another way?

Thank you,

Alexandre

0 Kudos
Reply

2,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

seems it supports raw format, one can look at example mipi raw data format in
https://community.freescale.com/message/386809#386809

Best regards
igor

0 Kudos
Reply