Capture three videos with 8 MP embedded CMOS sensors (with CSI2 output) with a i.MX6UL ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capture three videos with 8 MP embedded CMOS sensors (with CSI2 output) with a i.MX6UL ?

986 Views
thomasgadn
Contributor II

For a project, I need to Connect three 8MP Cameras with a CSI2 output to a i.MX6UL. Although I know that the i.MX6UL only supports 24 Bit Parallel CSI I hope there is a way to do that. 

I was thinking to MUX the three cameras with MIPI CSI2 MUX and then use a CSI2 to 24BIT Parallel bridge for connecting it to the controller, would it work? 

Otherwise, I was thinking to use three MIPI CSI2 to USB 2.0 bridge and use the two USB 2.0 PHY ports. 

Any recommendations to handle this would be great!

Thank you,

Tom

Labels (2)
1 Reply

924 Views
joanxie
NXP TechSupport
NXP TechSupport

I dont' think imx6ul can support 3-8MP camera, refer to the overview, imx6 can support up to 200M, if you use 3-8mp camera, should not be only 200M