Hi all,
I read this morning in the User's guide for the iMX.51 that "The WVGA board will support the following display interfaces: CPT 7” WVGA with resistive touch screen, CPT 5.7” VGA with resistive touch screen, Seiko 4.3” WVGA with resistive or capacitive touch screen and 18-Bit LVDS interface without touch screen."
I want a capacitive touch screen that can run on this board, but have been unable to find where I can purchase the above mentioned Seiko board with a capacitive touch screen. Does anyone have any ideas where I could find it, or if there are any other capacitive touchscreens that work well on the iMX51?