Capacitive Touch Screen for iMX.51

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capacitive Touch Screen for iMX.51

1,231 Views
AndrewBlack
Contributor I

Hi all,

I read this morning in the User's guide for the iMX.51 that "The WVGA board will support the following display interfaces: CPT 7” WVGA with resistive touch screen, CPT 5.7” VGA with resistive touch screen, Seiko 4.3” WVGA with resistive or capacitive touch screen and 18-Bit LVDS interface without touch screen."

I want a capacitive touch screen that can run on this board, but have been unable to find where I can purchase the above mentioned Seiko board with a capacitive touch screen. Does anyone have any ideas where I could find it, or if there are any other capacitive touchscreens that work well on the iMX51?

Tags (1)
0 Kudos
Reply
1 Reply

1,015 Views
mbp
Contributor V

Did you ever find a solution?

..or a resistive to capacitive adapter or Mx51 driver than allows add-on support for Capacitive touch?

thanks,

mike

0 Kudos
Reply