Cannot use low audio sample rates on imx28evk with 3.14.19 kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot use low audio sample rates on imx28evk with 3.14.19 kernel

2,065 Views
CraigMcQueen
Contributor III

I'm testing the 3.14.19 kernel on imx28evk, with a Yocto build that uses the linux-fslc kernel provider.

If I try to play or record at 8 kHz or 11.025 kHz, I get an error message:

# aplay test_8k.wav

[ 6168.910201] mxs_evk_startup: Skipped programming wolfson codec

Playing WAVE 'test_8k.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Mono

[ 6168.941211] sgtl5000 0-000a: Invalid mclk frequency: 4.096MHz

[ 6168.947047] mxs-sgtl5000 sound.11: ASoC: machine hw_params failed: -22

aplay: set_params:1145: Unable to install hw params:

...

For an 8 kHz sample rate, I get

Invalid mclk frequency: 4.096MHz

For 11.025 kHz sample rate, I get

Invalid mclk frequency: 5.644MHz

Looking in the code (/sound/soc/mxs/mxs-sgtl5000c), I see:

     /* Sgtl5000 sysclk should be >= 8MHz and <= 27M */

     if (mclk < 8000000 || mclk > 27000000) {

          dev_err(codec_dai->dev, "Invalid mclk frequency: %u.%03uMHz\n",

               mclk / 1000000, mclk / 1000 % 1000);

          return -EINVAL;

     }

But a sysclk constraint of 8 to 27 MHz only applies if the supplied clock is asynchronous to the frame clock, and the internal clock is being generated by PLL. I assume the PLL isn't being used. So can this constraint be relaxed?

Labels (2)
Tags (1)
0 Kudos
Reply
5 Replies

1,352 Views
fabio_estevam
NXP Employee
NXP Employee

Craig,

You are right that the 8-27MHz constraint does not apply when the sgtl5000 codec is slave.

I will prepare some patches to fix it, then will post at alsa-devel with you on Cc.

Thanks for reporting.

1,352 Views
fabio_estevam
NXP Employee
NXP Employee

Just tested playback of a 8k wav file and it works fine on 3.18-rc4:

root@freescale /home$ aplay mono_8k.wav

Playing WAVE 'mono_8k.wav' : Unsigned 8 bit, Rate 8000 Hz, Mono

0 Kudos
Reply

1,352 Views
CraigMcQueen
Contributor III

I've just tried it myself on a 3.18-rc4 kernel, but didn't get the same results as you. I got the same error as I previously got with the 3.14 kernel.

Maybe your device is using an ALSA asoundrc that is using plug or rate plugins to convert to a different sampling rate. Try using -D hw:0,0 option. First of all, I wouldn't expect a mono file to work, since the hardware needs 2 channels. E.g. I get:

# aplay -D hw:0,0 mono_8k.wav

Playing WAVE 'mono_8k.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Mono

aplay: set_params:1239: Channels count non available

But if you try a stereo file, then I expect you would get the invalid mclk frequency error:

# aplay -D hw:0,0 stereo_8k.wav

Playing WAVE 'stereo_8k.wav' : S[ 3718.857813] sgtl5000 0-000a: Invalid mclk frequency: 4.096MHz

igned 16 bit Little Endi[ 3718.865460] mxs-sgtl5000 sound: ASoC: machine hw_params failed: -22

an, Rate 8000 Hz, Stereo

aplay: set_params:1297: Unable to install hw params:

ACCESS:  RW_INTERLEAVED

FORMAT:  S16_LE

SUBFORMAT:  STD

SAMPLE_BITS: 16

FRAME_BITS: 32

CHANNELS: 2

RATE: 8000

...

0 Kudos
Reply

1,352 Views
fabio_estevam
NXP Employee
NXP Employee

Craig,

Please share your two wav files, so that I can test them here.

0 Kudos
Reply

1,352 Views
CraigMcQueen
Contributor III

I'm attaching 3 files.

0 Kudos
Reply