Cannot turn of Ethernet Chip 8720 using energy detect power down mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot turn of Ethernet Chip 8720 using energy detect power down mode

709 Views
nishigandhapati
Contributor II

Hello Everyone,

This question is related to ethernet phy driver.

We are using Android Nougat 7.1.2

We have SMSC ethernet chip LAN8720.

We have enabled the energy detect power down mode by enabling bit MII_LAN83C185_MODE_POWERDOWN of

MII_LAN83C185_CTRL_STATUS register.

Still when ethernet cable is not connected and ENERGYON bit is off, the chip is always on (the transceiver is always powered on) .

Have you seen this issue ?

All inputs are greatly appreciated.

Thank you very much

Nishi

Tags (2)
0 Kudos
1 Reply

660 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nishi

there are some patches and workarounds on web regarding that feature

https://lkml.org/lkml/2015/8/14/73 

phy: SMSC device Energy Detect power-down mode - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos