Cannot get Dual Video to Work!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot get Dual Video to Work!!

5,643 次查看
PaulDeMetrotion
Senior Contributor I

I have a custom BSP with an i.MX6Q wroking fine. I support HDMI video and two LVDS channels but cannot ever get HDMI and LVDS to work simultaneously. Whichever video source I map to fb0 works fine but I never get the second video source to work. Here is my boot command line. With this command line I get HDMI video but not LVDS. If I switch fb0 and fb1, I then get LVDS video but not HDMI.

console=ttymxc0,115200 root=/dev/mmcblk0p1 rootwait rw ip=dchp video=mxcfb0:dev=hdmi,1280x720M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RG666

Here is my xorg.conf file:

Section "InputDevice"
        Identifier      "Generic Keyboard"
        Driver          "kbd"
        Option          "XkbRules"      "xorg"
        Option          "XkbModel"      "pc105"
        Option          "XkbLayout"     "us"
EndSection

Section "InputDevice"
        Identifier      "Configured Mouse"
        Driver          "mouse"
        Option          "CorePointer"
EndSection

Section "Device"
        Identifier      "i.MX Accelerated Framebuffer Device 0"
        Driver          "vivante"
        Option          "fbdev"         "/dev/fb0"
        Option          "vivante_fbdev" "/dev/fb0"
        Option          "HWcursor"      "false"
EndSection

Section "Device"
        Identifier      "i.MX Accelerated Framebuffer Device 1"
        Driver          "vivante"
        Option          "fbdev"         "/dev/fb1"
EndSection

Section "Monitor"
        Identifier      "Configured Monitor 0"
EndSection

Section "Monitor"
        Identifier      "Configured Monitor 1"
EndSection

Section "Screen"
        Identifier      "Screen 0"
        Monitor         "Configured Monitor 0"
        Device          "i.MX Accelerated Framebuffer Device 0"
EndSection

Section "Screen"
        Identifier      "Screen 1"
        Monitor         "Configured Monitor 1"
        Device          "i.MX Accelerated Framebuffer Device 1"
EndSection

Section "ServerLayout"
        Identifier      "Xinerama Layout"
        Screen          "Screen 0"
        Screen          "Screen 1"

EndSection

Section "ServerFlags"
        Option          "Xinerama"      "true"
EndSection

If I only have Screen 0, it works fine. If I add any reference to Screen 1, I get no video on either monitor.

Does all of this look correct? Any help will be grealty appreciated.

标签 (3)
13 回复数

4,062 次查看
PaulDeMetrotion
Senior Contributor I

Nobody has any dual video experience. Any help will be appreciated. What causes the message "Screen 1 deleted because of no matching config section"?

0 项奖励
回复

4,062 次查看
GaoJianzhong
Contributor IV

Hi

Now i have a same problem when to use two diaplay on i.mx6q board.

My system is ubuntu。 And i what to use LVDS as the primary dispaly and use HDMI as the second one.

My u-boot's kernel parameters is bellow:

video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24

And my x window configure file is as bellow:

Section "InputDevice"

        Identifier      "Generic Keyboard"

        Driver          "kbd"

        Option          "XkbRules"      "xorg"

        Option          "XkbModel"      "pc105"

        Option          "XkbLayout"     "us"

EndSection

Section "InputDevice"

        Identifier      "Configured Mouse"

        Driver          "mouse"

        Option          "CorePointer"

EndSection

Section "Device"

        Identifier      "LVDS"

       Driver          "vivante"

        Option          "fbdev"         "/dev/fb0"

       Option          "vivante_fbdev" "/dev/fb0"

       Option          "HWcursor"      "false"

EndSection

Section "Device"

        Identifier      "HDMI"

        Driver          "fbdev"                        ///////////////  If i use "vivante", X window start will failed, it seems that "vivante" not support two display?

        Option          "fbdev"         "/dev/fb2"

EndSection

Section "Monitor"

        Identifier      "LVDS Monitor"

EndSection

Section "Monitor"

        Identifier      "HDMI Monitor"

EndSection

Section "Screen"

        Identifier      "LVDS Screen"

        Monitor         "LVDS Monitor"

        Device          "LVDS"

EndSection

Section "Screen"

        Identifier      "HDMI Screen"

        Monitor         "HDMI Monitor"

        Device          "HDMI"

EndSection

Section "ServerLayout"

        Identifier      "Dual Layout"

        Screen 0        "LVDS Screen"

        Screen 1        "HDMI Screen" RightOf "LVDS Screen"

        Option          "Xinerama"  "on"

EndSection

Then i get the two display worked, But somthing is wrong.

On the left of HDMI display there is a copy of lvds.

Is my settings wrong?

Do you know about this?

Thank youLVDS.jpgHDMI.jpg

0 项奖励
回复

4,062 次查看
PaulDeMetrotion
Senior Contributor I

Update: After reviewing the Xorg.0.log file, I found the following error:

Screen 1 deleted because of no matching config section.

This is obviously why I cannot see the second screen in the Ubuntu GUI. Does anybody have any ideas what the missing config section is?

0 项奖励
回复

4,062 次查看
PaulDeMetrotion
Senior Contributor I

Update: I still do not have dual video during uImage boot or when the GUI is displayed. I am able to use gstreamer to display a test pattern and an mp4 video on both displays. I can even run videos on both displays at the same time.

Obviously both monitors are usable so why does the secondary monitor not function early in the boot cycle or when the GUI is displayed? Should I see penguins on both displays during boot? Should I be able to run my GUI using both monitors?

0 项奖励
回复

4,062 次查看
PaulDeMetrotion
Senior Contributor I

Update: In my custom board configuration file I had disabled the imx6q_add_v4l2_output(0) call and when I added it again, the video improved. I still do not get dual video but the second monitor (LVDS) is in sync and appears usable but is just a black screen. This is my new command line:

 

console=ttymxc0,115200 root=/dev/mmcblk0p1 rootwait rw ip=dchp video=mxcfb0:dev=hdmi,1280x720M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 ldb=sin0

This is my last attempt at a xorg.conf file:

Section "InputDevice"
        Identifier      "Generic Keyboard"
        Driver          "kbd"
        Option          "XkbRules"      "xorg"
        Option          "XkbModel"      "pc105"
        Option          "XkbLayout"     "us"
EndSection

Section "InputDevice"
        Identifier      "Configured Mouse"
        Driver          "mouse"
        Option          "CorePointer"
EndSection

Section "Device"
        Identifier      "i.MX Accelerated Framebuffer Device 0"
        Driver          "vivante"
        Screen          0
        Option          "fbdev"         "/dev/fb0"
        Option          "vivante_fbdev" "/dev/fb0"
        Option          "HWcursor"      "false"
EndSection

Section "Device"
        Identifier      "i.MX Accelerated Framebuffer Device 1"
        Driver          "vivante"
        Screen          1
        Option          "fbdev"         "/dev/fb1"
        Option          "vivante_fbdev" "/dev/fb1"
        Option          "HWcursor"      "false"
EndSection

Section "Monitor"
        Identifier      "Configured Monitor 0"
EndSection

Section "Monitor"
        Identifier      "Configured Monitor 1"
EndSection

Section "Screen"
        Identifier      "Screen 0"
        Device          "i.MX Accelerated Framebuffer Device 0"
        Monitor         "Configured Monitor 0"
EndSection

Section "Screen"
        Identifier      "Screen 1"
        Device          "i.MX Accelerated Framebuffer Device 1"
        Monitor         "Configured Monitor 1"

Section "ServerLayout"
        Identifier      "Xinerama Layout"
        Screen          0 "Screen 0" 0 0
        Screen          1 "Screen 1" RightOf "Screen 0"
        InputDevice     "Generic Keyboard"
        InputDevice     "Configured Mouse"
        Option          "Xinerama"      "on"
EndSection

Anybody know what could be wrong?

0 项奖励
回复

4,062 次查看
LeonardoSandova
Specialist I

have you tried ldb=dul0/1 ? Regarding the xorg.conf, what are the related kernel logs when xserver loads?

4,062 次查看
kevinlee90008
Contributor I

I have same situation like Paul and I already try ldb=dul0/1 and any kernel parameter in the release note.My touch can work but LVDS got black screen. Could anyone tell me why?  and I also get HDMI video but not LVDS. If I switch fb0 and fb1, I then get LVDS video but not HDMI. This is my command line setting :

bootargs=console=ttymxc0,115200 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 ldb=dul0 fbmem=28M,10M

0 项奖励
回复

4,062 次查看
PaulDeMetrotion
Senior Contributor I

What board are you using?

0 项奖励
回复

4,062 次查看
kevinlee90008
Contributor I

imx 6Q

0 项奖励
回复

4,062 次查看
LeonardoSandova
Specialist I

Paul,

I think you need to add the 'ldb' kernel command line parameter, take at look at the release notes for more documentation.

Leo

0 项奖励
回复

4,062 次查看
PaulDeMetrotion
Senior Contributor I

Don't I already have that - video=mxcfb1:dev=ldb,LDB-XGA,if=RG666 - or is there another parameter required?

0 项奖励
回复

4,062 次查看
IvicaEftimovski
Contributor III

I think Leonardo is right. I don't have the i.MX6, but in my i.MX5 QSB I have the line below when I want two displays:

"video=mxcdi0fb:RGB666,800x480@60 di0_primary ldb=di0 video=mxcdi1fb:RGB666,800x480@60 ldb=di1"

0 项奖励
回复

4,062 次查看
LeonardoSandova
Specialist I

It is another parameter. I am trying to copy & paste the release note documentation but the paste formatting is so bad, so look at the document for this.