Cannot find kernel branch rel_imx_5.4.3-1.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot find kernel branch rel_imx_5.4.3-1.0.0

1,480 次查看
marcocontenti
Contributor II

Hello,

I am trying to build kernel 5.4.3 for i.MX family following section 2.1.1 of i.MX Porting Guide, Rev. L5.4.3_1.0.0 I just downloaded, along with Release notes, etc. all referring to rev. 5.4.3_1.0.0 of the i.MX kernel.

After cloning the kernel repo from https://source.codeaurora.org/external/imx/linux-imx I am supposed to find a rel_imx_5.4.3-1.0.0 branch to check out. Actually this branch doesn't exist in the repository. I can find instead a rel_imx_5.4.3-2.0.0 branch, but I am not sure I can use it.

So, which is the right branch to check out?

Thanks,

Marco

标签 (1)
0 项奖励
回复
2 回复数

1,352 次查看
marcocontenti
Contributor II

Answering myself, I downloaded the Yocto source code for 5.4.3-1.0.0 and found out in the kernel recipe that the correct branch should be "lf-5.4.y". There is also a tag "lf-5.4.y-1.0.0" pointing to the same commit with hash "f8118585ee3c7025265b28985fdfe0af96a84466". Not so self-evident as in past releases.

Marco

1,352 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Marco,

I’m glad that you found out the cause of this problem. My apologies for the confusion. It is a departure from previous naming conventions (and this is indeed not expressly stated on the documentation). Hopefully your post will help other Community users.

Regards,

0 项奖励
回复