Cannot bring up Murata wifi module on MYD-JX8MPQ having iMX8MPLUS chipset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot bring up Murata wifi module on MYD-JX8MPQ having iMX8MPLUS chipset

399 Views
sanum19
Contributor II

Im trying to interface murata(SDIW612) wifi module in n mydjx8mpq. The wifi interface is SDIO alone on the board.Kernel is 5.10.9...

I tried following the steps in nxp's bringup documents:

 |

 |

 \/

root@imx8mqevk:~# nano /lib/firmware/nxp/wifi_mod_para.conf
Content of the configuration file:

SDIW612 = {
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode=7
fw_name=nxp/sduart_nw61x_v1.bin.se
}
• Load the modules in the kernel
root@imx8mqevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf

<>

Couldnt find sduart_nw61x_v1.bin.se - this particular file inside /lib/firmware/nxp. Where can i get it for kernel 5.10.9?

 

0 Kudos
4 Replies

371 Views
sanum19
Contributor II

expected logexpected loglog fom my devicelog fom my device

shaun_wu THanks for the reply.

Even after i tried adding these files. Couldnt laod wlan in my setup.

when i does - modprobe moal mod_para=nxp/wifi_mod_para.conf : The above SS is what  the expected log as per the documentation and dmesg log that, i get.

The kernel im using is 5.10.9. In the link you shared me the req file is found under branch 6.1.36 .Does that mean IW612 doesnt have support on kernel 5.10? 

 

0 Kudos

366 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @sanum19 

 

You could use 

ifconfig -a

 to check if mlan0 are enabled successfully. 

 

Best Regards

Shaun

358 Views
sanum19
Contributor II

mlan0 or wlan0 interfaces are not coming up on "ifconfig -a". Also the dmesg log shows no error. This is were i'm troubled with.

The module is inserted and are loaded in mmc0. Here is the log :

$ dmesg | grep -i mmc0

[ 1.715449] mmc0: CQHCI version 5.10
[ 3.053116] mmc0: CQHCI version 5.10
[ 3.118576] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 3.199001] mmc0: new ultra high speed SDR104 SDIO card at address 0001

$ dmesg | grep -i mmc1

[ 1.715792] mmc1: CQHCI version 5.10
[ 3.054795] mmc1: CQHCI version 5.10
[ 3.088605] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 3.257302] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.404820] mmc1: new ultra high speed SDR104 SDHC card at address 0007
[ 3.412692] mmcblk1: mmc1:0007 SD16G 14.5 GiB

$ dmesg | grep -i mmc2
[ 1.719506] mmc2: CQHCI version 5.10
[ 1.751686] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 1.917692] mmc2: Command Queue Engine enabled
[ 1.922184] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 1.929934] mmcblk2: mmc2:0001 H8G4a2 7.28 GiB
[ 1.934600] mmcblk2boot0: mmc2:0001 H8G4a2 partition 1 8.00 MiB
[ 1.940767] mmcblk2boot1: mmc2:0001 H8G4a2 partition 2 8.00 MiB
[ 1.946930] mmcblk2rpmb: mmc2:0001 H8G4a2 partition 3 4.00 MiB, chardev (235:0)

shaun_wuCould you please give me guidance to how to troubleshoot this?

0 Kudos

384 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello 

 

You can download iw61x firmware here: imx-firmware/nxp/FwImage_IW612_SD at lf-6.1.36_2.1.0 · nxp-imx/imx-firmware · GitHub

 

Best Regards

Shaun