Cannot boot imx28evk from SD card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot boot imx28evk from SD card

1,346件の閲覧回数
swainsun
Contributor I

Hi Bros,

 

I'm a new guy of embeded dev, using i.mx28evk.

 

I fellow the step by step doc to config the vm, installed ubuntu 10.04 on my vmware. I downloaded the L2.6.35_10.12.01_SDK_source_bundle, and fellow the instructions of the guide doc. The ltib installed quickly, and during the ./ltib process, the required pkgs were installed and solved the mtd-utils pkg build failed issue. And normally, i used the mk_mx28_sd script write the boot stream, fs, kernel to the SD card. But error existed when i power the board on.

 

Here goes the error,

4276_4276.png282F0669-10C4-47A7-BB80-0A9CD5372B55.png

 

And attched is my config file, anyone can help me?

 

Thanks, thanks.

Original Attachment has been moved to: imx28.config.zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,180件の閲覧回数
Yuri
NXP Employee
NXP Employee

As I remember the mk_mx28_sd script does not work correctly under Ubuntu 12.04.
Please try using the MFG to deploy images to SD.

0 件の賞賛
返信

1,180件の閲覧回数
swainsun
Contributor I

Thanks for your quick replay, but i dont use Ubuntu 12.04, using Ubuntu 10.04.

0 件の賞賛
返信