Cannot Find the "i.MX Linux User's Guide"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot Find the "i.MX Linux User's Guide"

5,193 Views
cbrust
Contributor III

The "i.MX Linux User's Guide" is referenced in several documents including the "Freescale Yocto Project User's Guide".  However, I am unable to locate this document anywhere.  Can someone direct me to the document? 

Here's the reference pulled from the Freescale Yocto Project User's Guide.

Appendix B References

For details on boot switches, see Section "How to Boot the i.MX Boards" in the

i.MX Linux User's Guide

For how to download images using U-boot, see Section "Downloading Images Using U-Boot" in the

i.MX Linux User's Guide

For how to set up an SD/MMC card, see Section "Preparing an SD/MMC Card to Boot" in the

i.MX Linux User's Guide

Labels (3)
0 Kudos
1 Reply

1,088 Views
igorpadykov
NXP Employee
NXP Employee

Hi Brust

Linux User Guide is included in Doc Bundle for each BSP (also please find it attached)

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------