Cann't tx/rx bytes by usart 3 on DART-MX8M board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cann't tx/rx bytes by usart 3 on DART-MX8M board

967 Views
user4users
Contributor I

Hello everyone.

 

I have DART-MX8M-MINI Evaluation Kit. And I want to send something via USART.

USART3 is free on this board.

 

I enabled USART3 in device tree. And when I am trying this cmd:

stty -F /dev/ttymxc2 -echo -onlcr 115200

 

I had got this:

 

[ 232.697916] imx-sdma 30bd0000.dma-controller: sdma firmware not ready!

[ 232.704455] imx-uart 30880000.serial: We cannot prepare for the RX slave dma!

[ 232.711815] imx-sdma 30bd0000.dma-controller: sdma firmware not ready!

[ 232.718351] imx-uart 30880000.serial: We cannot prepare for the TX slave dma!

 

I can’t transmit or receive bytes.

 

What I am doing wrong?

I tried to change status dma in device tree but this did not help me.

 

I am using Debian 10.6 and Linux imx8mm-var-dart 4.19.35.

 

Build image by this instructions:

https://variwiki.com/index.php title=Debian_Build_Release&release=RELEASE_BUSTER_V2.1_DART-MX8M-MINI

0 Kudos
Reply
1 Reply

959 Views
igorpadykov
NXP Employee
NXP Employee

Hi user4users

 

for uart usage for that board may be useful to look at

https://variwiki.com/index.php?title=DART-MX8M_UART&release=RELEASE_ZEUS_V1.1_DART-MX8M-MINI

In general this board was designed and supported by variscite, suggest to post issue on

its tech support  https://www.variscite.com/support/

 

Best regards
igor

 

 

0 Kudos
Reply