Can you get uboot using ksz9031?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can you get uboot using ksz9031?

942件の閲覧回数
aszsz123
Contributor I

Can you get uboot using ksz9031?

My board specifications use mx6dl, ddr3 1g, ksz9031, 512mb nand.
Finally, I intend to install uboot in the nand.

Somebody help me!

ラベル(4)
0 件の賞賛
返信
1 返信

879件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Seyeon

one can look at

Porting KSZ9031 to i.MX BSP 

https://community.nxp.com/thread/352309 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信