Can we use i.MX6SDL USB PHY setting for USB certification in normal operation also?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we use i.MX6SDL USB PHY setting for USB certification in normal operation also?

399件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL USB PHY.

Please see chapter 66.2.6 in IMX6SDLRM (Rev.2).

This chapter says the recommended register setting for USB certification.

I think this setting can be used for normal operation if the eye pattern is good.

Is this understanding correct?

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(2)
0 件の賞賛
1 返信

339件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes, this understanding is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛