Can we use i.MX6SDL USB PHY setting for USB certification in normal operation also?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use i.MX6SDL USB PHY setting for USB certification in normal operation also?

400 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL USB PHY.

Please see chapter 66.2.6 in IMX6SDLRM (Rev.2).

This chapter says the recommended register setting for USB certification.

I think this setting can be used for normal operation if the eye pattern is good.

Is this understanding correct?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (2)
0 Kudos
1 Reply

340 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes, this understanding is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos