Can we use i.MX6DQ IPU unpacking capability when input format is generic data.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use i.MX6DQ IPU unpacking capability when input format is generic data.

Jump to solution
1,590 Views
satoshishimoda
Senior Contributor I

Hi community,

Our patner have a question about i.MX6DQ IPU.
Please see page 2732 in IMX6DQRM Rev.2.
It says "Unpacking and companding capabilities are provided for up to two streams (either through same or different interfaces), while the other ones are treated as generic data."
Then, can we use this function when input data as "generic data" (when CSIx_SENS_DATA_FORMAT = 011b)?


Best Regards,
Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
1,434 Views
Yuri
NXP Employee
NXP Employee

Unpacking and companding capabilities are not provided for the generic data.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
1,435 Views
Yuri
NXP Employee
NXP Employee

Unpacking and companding capabilities are not provided for the generic data.

Regards,

Yuri.

0 Kudos
Reply
1,434 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

I found the packing (companding) function in chapter 37.4.3.7 and Table 37-17 in IMX6DQRM Rev.3.

Bayer and Generic input data seem to be able to compand also according to this section, is this wrong?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,434 Views
Yuri
NXP Employee
NXP Employee

Hi,

  Basically, data unpacking means that format of data is known (say, R8G8B8).

For generic data, format is not predefined. The Table 37-17 states that generic

are treated just as bytes or 16-bit words, based on port size.

Regards,

Yuri.

0 Kudos
Reply