Can we test DDR3 during booting from SD Card?

cancel
Showing results for 
Search instead for 
Did you mean: 

Can we test DDR3 during booting from SD Card?

Jump to solution
377 Views
DeepakNaik
Contributor I

My bootloader is in SD card card? I want to check the feasibility to test DDR3 by booting  primary boot loader from sd card into internal SRAM and testing DDR3. Downloading the next boot loader into DDR3

-Deepak

0 Kudos
1 Solution
216 Views
VladanJovanovic
NXP Employee
NXP Employee

That should be possible. I believe i later versions of u-boot, special "plugin" function is used during boot to initialize memory. You may add your DDR3 test to that part of code, and still leave internal ROM to load the rest of the bootloader to memory after you've done your tests.

U-boot code related to this should be in (approximately): board/freescale/mx53_loco/flash_header.S.

View solution in original post

0 Kudos
1 Reply
217 Views
VladanJovanovic
NXP Employee
NXP Employee

That should be possible. I believe i later versions of u-boot, special "plugin" function is used during boot to initialize memory. You may add your DDR3 test to that part of code, and still leave internal ROM to load the rest of the bootloader to memory after you've done your tests.

U-boot code related to this should be in (approximately): board/freescale/mx53_loco/flash_header.S.

0 Kudos