Can we interface MT25QL02GCBB8E12-0SIT in QSPI mode with i.MX6 Quad or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we interface MT25QL02GCBB8E12-0SIT in QSPI mode with i.MX6 Quad or not?

721 Views
sagar_kumar
Contributor I

Hi

Can we interface XIP NOR FLASH MT25QL02GCBB8E12-0SIT (2Gb- 256Mx8) in QSPI mode with i.MX6 Quad or not?

Labels (1)
0 Kudos
Reply
1 Reply

659 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sagar

i.MX6Q does not support boot from qspi nor, supported boot devives are described in

Chapter 8 System Boot i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply