Hello,
I noticed that the Sabre Lite board supplies 1.2V to it's VDDARM input. The IMX6Q datasheet says that the processor needs a minimum of 1.35V to run at 1GHz in LDO mode and 1.225V minimum to run in LDO bypass mode. It appears that the Sabre Lite wouldn't support the 1GHZ ARM Clock frequency, is this true?
1. Does Sabre Lite support operation at 1GHz?
2. Does the Sabre Lite run in LDO Bypassed mode?
I assume the answer to this question would also apply to the maximum SOC frequency
Thanks,
KBell