Can the M40 core in imx8qm use hdmi-tx port for display?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the M40 core in imx8qm use hdmi-tx port for display?

826 Views
jinchen1227
Contributor II

There is a hdmi-tx port on imx8qm-mek board, can the M4 core0 use this port for display?

I find this port is connect with dpu1, now I can use dpu1 and it's LVDS port to display.

Can I use both HDMI-tx and LVDS port to display on two screens?

Tags (2)
0 Kudos
2 Replies

759 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Chen,

You can  use the lvds and hdmi for dual display, but the M4 need to be at LVDS.

Regards

0 Kudos

759 Views
jinchen1227
Contributor II

Thank you!

Another question, can the M4 core use both mipi and lvds at the same time for dual display at the same time?

0 Kudos