Can the IMX6Q output the LVDS video in only one pair Differential signal?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can the IMX6Q output the LVDS video in only one pair Differential signal?

跳至解决方案
703 次查看
翔李
Contributor IV

Hi, can the IMX6Q output the LVDS video in only one pair Differential signal?  Because the monitor which the IMX6Q board connects,has only one pari Differential signal interface. Thanks.

标签 (1)
0 项奖励
回复
1 解答
583 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

unfortunately not, this is fixed in hardware. From

IMX6DQRM Table 39-1. LDB - Block Description :

LDB has 2 channel serializers. The serializer does parallel to serial conversion 7:1 to

3 or 4 data lines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
584 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

unfortunately not, this is fixed in hardware. From

IMX6DQRM Table 39-1. LDB - Block Description :

LDB has 2 channel serializers. The serializer does parallel to serial conversion 7:1 to

3 or 4 data lines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复