Can the IMX6Q output the LVDS video in only one pair Differential signal?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the IMX6Q output the LVDS video in only one pair Differential signal?

ソリューションへジャンプ
1,284件の閲覧回数
翔李
Contributor IV

Hi, can the IMX6Q output the LVDS video in only one pair Differential signal?  Because the monitor which the IMX6Q board connects,has only one pari Differential signal interface. Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,164件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

unfortunately not, this is fixed in hardware. From

IMX6DQRM Table 39-1. LDB - Block Description :

LDB has 2 channel serializers. The serializer does parallel to serial conversion 7:1 to

3 or 4 data lines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,165件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

unfortunately not, this is fixed in hardware. From

IMX6DQRM Table 39-1. LDB - Block Description :

LDB has 2 channel serializers. The serializer does parallel to serial conversion 7:1 to

3 or 4 data lines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信