Hello,
I want a signal to be high when the processor is in standby mode. Can imx6qp assign a signal from the GPIO while in low power mode? I looked at the relevant docs but couldn't find an answer. Glad if you help
Thanks, regards
解決済! 解決策の投稿を見る。
Hi Celile
gpio pad settings (like pull-up) are retained in low power modes, they can not be configured specific
for some low power mode, one can look at for example MX6QDL_PAD_EIM_A25__GPIO5_IO02 0x000b1
bits PUE,PKE,PUS described in sect.36.4.227 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_EIM_ADDR25)
i.MX 6Dual/6Quad Applications Processor Reference Manual
AN5078 Influence of Pin Setting on System Function and Performance
Best regards
igor
Hi Celile
gpio pad settings (like pull-up) are retained in low power modes, they can not be configured specific
for some low power mode, one can look at for example MX6QDL_PAD_EIM_A25__GPIO5_IO02 0x000b1
bits PUE,PKE,PUS described in sect.36.4.227 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_EIM_ADDR25)
i.MX 6Dual/6Quad Applications Processor Reference Manual
AN5078 Influence of Pin Setting on System Function and Performance
Best regards
igor